SNOU211 November 2024
The EVM is divided into 2 sections: the controller section and the sensor breakout section. The sensor breakout section can be detached to use the sensor in the following scenarios:
Figure 2-1 highlights the EVM sections as well as some components that must be identified by the user to understand the purpose and use. The components are further explained in detail in the sections below.