SNOU211 November 2024
The Data Capture tab reports the temperature from the TMP113 device included on the TMP113EVM. By default, once the EVM is connected and the GUI is loaded and running properly, the device starts in continuous conversion mode and the MCU starts polling the device. The conversion results are automatically reported and displayed in the Data tab graph.
On the right side of this tab, the user can view the latest temperature read value. There is also a chart controls box which allows the user to:
The Alert Config box allows the user to easily configure the alert functionality settings of the TMP113 such as polarity, mode, and limits. The limits can be written on the left box in decimal format, and the corresponding hexadecimal value is automatically displayed in the right box for reference. Once selected or updated, all of the settings are written automatically to the TMP113 by the MCU.
Figure 3-5 Data Capture