SNOU211 November 2024
The TMP113EVM has an Address Selection portion of the breakout section, which has footprints for 4 solderable jumper resistors. The default EVM configuration connects the ADDR pin to GND via jumper R01. The jumper can be moved to the R02, R03, or R04 footprint to connect the ADDR pin to SDA, SCL, or VDD, respectively. See Table 2-2 for the corresponding I2C address for each ADDR pin configuration. Take care to only install 1 jumper at a time to avoid shorts.
When interfacing the ADDR pin on the sensor breakout section to an external connection, all jumpers must be removed first to avoid shorts. Then, a header pin or wire can be soldered to connect ADDR to GND, VDD, SDA, or SCL through the user's custom connection.
| TARGET I2C ADDRESS | ADDR PIN CONNECTION |
|---|---|
| 1001000 | GND |
| 1001001 | VDD |
| 1001010 | SDA |
|
1001011 |
SCL |