SPRAC21A June 2016 – June 2019 OMAP-L132 , OMAP-L138 , TDA2E , TDA2EG-17 , TDA2HF , TDA2HG , TDA2HV , TDA2LF , TDA2P-ABZ , TDA2P-ACD , TDA2SA , TDA2SG , TDA2SX , TDA3LA , TDA3LX , TDA3MA , TDA3MD , TDA3MV
The following bar graphs show the impact of the improvement in bandwidth of single transfer controller System EDMA, DSP EDMA, and EVE EDMA for interleaved EMIF versus non-interleaved EMIF. The interleaving leads to lesser DDR page opens and closes, which leads to improvement of the individual EMIF performances. Because two EMIFs are used for any data transfer greater than 128 Bytes, the total bandwidth available for the initiators also increases significantly. Note that in the following data (for the interleaved case, especially), the total utilization of the available EMIF bandwidth is less as the system is now initiator bottlenecked; that is, the initiator (EDMA TC) requests do not generate the fill of the EMIF command FIFOs.
Figure 51. System EDMA Single Transfer Controller
Figure 52. DSP EDMA Single Transfer Controller
Figure 53. EVE EDMA Single Transfer Controller