SPRAC77E January 2022 – February 2022 TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
The example projects can be found in the directory shown in Table 6-1. The example projects use the API library projects that are described in Section 7.
| C:\ti\c2000\C2000Ware_MotorControl_SDK_[version]\ | Default install location for the SDK. ([SDK]) |
| [SDK]\solutions\boostxl_posmgr\ | Device-specific solutions base install directory ([pto_base]) |
| [pto_base]\shared\source | Source code that is device independent and used across different device examples. |
| [pto_base]\[device]\source | Source code for the example projects. Includes both .c and .syscfg files. |
| [pto_base]\[device]\include | Example-specific header files. |
| [pto_base]\[device]\ccs\[pto_example] | Code Composer Studio (CCS) projectspec files. Used to import the project into your CCS workspace. |
| [pto_base]\[device]\cmd | Example project linker command files (.cmd). |