SPRADL4 January   2025 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Differences Between EEPROM and On-Chip Flash
  6. 3 Overview
    1. 3.1 Basic Concepts
    2. 3.2 Single-Unit Method
    3. 3.3 Ping-Pong Method
    4. 3.4 Creating EEPROM Sections (Pages) and Page Identification
  7. 4 Software Description
    1. 4.1 Software Functionality and Flow
  8. 5 Single-Unit Emulation
    1. 5.1 User Configuration
      1. 5.1.1 EEPROM_Config.h
      2. 5.1.2 F29H85x_EEPROM.c
    2. 5.2 EEPROM Functions
      1. 5.2.1 Initialization and Setup Functions
        1. 5.2.1.1 Configure_Device
        2. 5.2.1.2 EEPROM_Config_Check
      2. 5.2.2 Page Mode Functions
        1. 5.2.2.1 EEPROM_GetValidBank
        2. 5.2.2.2 EEPROM_UpdateBankStatus
        3. 5.2.2.3 EEPROM_UpdatePageStatus
        4. 5.2.2.4 EEPROM_UpdatePageData
        5. 5.2.2.5 EEPROM_Write_Page
      3. 5.2.3 64-Bit Mode Functions
        1. 5.2.3.1 EEPROM_64_Bit_Mode_Check_EOS
        2. 5.2.3.2 EEPROM_Write_64_Bits
      4. 5.2.4 Functions Used in Both Modes
        1. 5.2.4.1 EEPROM_Erase
        2. 5.2.4.2 EEPROM_Read
      5. 5.2.5 Utility Functions
        1. 5.2.5.1 EEPROM_Write_Buffer
        2. 5.2.5.2 Erase_Bank
        3. 5.2.5.3 Set_Protection_Masks
        4. 5.2.5.4 Configure_Protection_Masks
        5. 5.2.5.5 Fill_Buffer
        6. 5.2.5.6 ClearFSMStatus
    3. 5.3 Testing Example
  9. 6 Ping-Pong Emulation
    1. 6.1 User-Configuration
      1. 6.1.1 EEPROM_PingPong_Config.h
      2. 6.1.2 F29H85x_EEPROM_PingPong.c
    2. 6.2 EEPROM Functions
      1. 6.2.1 Initialization and Setup Functions
        1. 6.2.1.1 Configure_Device
        2. 6.2.1.2 EEPROM_Config_Check
      2. 6.2.2 Page Mode Functions
        1. 6.2.2.1 EEPROM_GetValidBank
        2. 6.2.2.2 EEPROM_UpdateBankStatus
        3. 6.2.2.3 EEPROM_UpdatePageStatus
        4. 6.2.2.4 EEPROM_UpdatePageData
        5. 6.2.2.5 EEPROM_Write_Page
      3. 6.2.3 64-Bit Mode Functions
        1. 6.2.3.1 EEPROM_64_Bit_Mode_Check_EOS
        2. 6.2.3.2 EEPROM_Write_64_Bits
      4. 6.2.4 Functions Used in Both Modes
        1. 6.2.4.1 EEPROM_Erase_Inactive_Unit
        2. 6.2.4.2 EEPROM_Read
        3. 6.2.4.3 EEPROM_Erase_All
      5. 6.2.5 Utility Functions
        1. 6.2.5.1 EEPROM_Write_Buffer
        2. 6.2.5.2 Erase_Bank
        3. 6.2.5.3 Configure_Protection_Masks
        4. 6.2.5.4 Set_Protection_Masks
        5. 6.2.5.5 Fill_Buffer
        6. 6.2.5.6 ClearFSMStatus
    3. 6.3 Testing Example
  10. 7 Application Integration
  11. 8 Flash API
    1. 8.1 Flash API Checklist
      1. 8.1.1 Flash API Do's and Do Not's
  12. 9 Source File Listing
  13. 10Troubleshooting
    1. 10.1 General
  14. 11Conclusion
  15. 12References

EEPROM_Config_Check

The EEPROM_Config_Check() function performs general error-checking and configures Write/Erase protection masks required by the Flash API. This function should be called before programming or reading from the emulated EEPROM Unit(s).

First, the function verifies that the Flash Bank selected for EEPROM Emulation is valid. On F29H85x, only the data flash is currently supported.

if (FLASH_BANK_SELECT != C29FlashBankFR4RP0StartAddress)
{
    return 0xFFFF;
}

Second, the validity of Flash Sectors selected for emulation is examined. This checks for:

  • If more Flash sectors have been selected for emulation than exist on the device, and if at least one flash sector has been selected

uint32_t NUM_EEPROM_SECTORS_1 = FIRST_AND_LAST_SECTOR[1] - FIRST_AND_LAST_SECTOR[0] + 1;

NUM_EEPROM_SECTORS = NUM_EEPROM_SECTORS_1;

if (NUM_EEPROM_SECTORS > NUM_FLASH_SECTORS || NUM_EEPROM_SECTORS == 0)
{
    return 0xEEEE;
}
  • Invalid combinations of the first and last Sectors selected for emulation
if (NUM_EEPROM_SECTORS > 1)
{
    if (FIRST_AND_LAST_SECTOR[1] <= FIRST_AND_LAST_SECTOR[0])
    {
        return 0xEEEE;
    }

    if (FIRST_AND_LAST_SECTOR[1] > NUM_FLASH_SECTORS - 1 || FIRST_AND_LAST_SECTOR[1] < 1)
    {
        return 0xEEEE;
    }
}
else if (FIRST_AND_LAST_SECTOR[0] > NUM_FLASH_SECTORS - 1 ||
         FIRST_AND_LAST_SECTOR[1] > NUM_FLASH_SECTORS - 1)
{
    return 0xEEEE;
}

If using Page Mode, the following will also be checked:

  • If the total size of EEPROM Banks + Pages will fit in the Flash Sectors selected
Bank_Size = WRITE_SIZE_BYTES*2 + ((EEPROM_PAGE_DATA_SIZE + WRITE_SIZE_BYTES*2) * NUM_EEPROM_PAGES);

uint32 Available_Words = NUM_EEPROM_SECTORS * FLASH_SECTOR_SIZE;

if (Bank_Size * NUM_EEPROM_BANKS > Available_Words)
{
    return 0xCCCC;
}

It will also warn you with the appropriate code if one of the following conditions is detected:

  • If space for one or more EEPROM Banks is left in Flash after configuring EEPROM Bank and Page size
if (Available_Words - (Bank_Size * NUM_EEPROM_BANKS ) >= Bank_Size)
{
    Warning_Flags += 1;
}
  • If each page consists of less than or equal to 64 bits (8 bytes) (this wastes space as the 64-Bit Mode could be used for the same effect, without the overhead of status codes)
if (DATA_SIZE <= WRITE_SIZE_BYTES)
{
    Warning_Flags += 2;
}
  • If using sectors in the 32-127 range and not using all eight sectors allocated to a single bit in the write protection mask, a warning is issued. Any unused sectors within group cannot be properly be protected from erase. For more information on write protection masks, see the F29H85x Flash API Reference Guide.

if (FIRST_AND_LAST_SECTOR[0] > 31 && FIRST_AND_LAST_SECTOR[1] > 31)
{

    if (NUM_EEPROM_SECTORS < 8)
    {
        Warning_Flags += 4;
    }



    else if ((FIRST_AND_LAST_SECTOR[0] % 8) != 0 || (FIRST_AND_LAST_SECTOR[1] + 1) % 8 != 0)
    {
        Warning_Flags += 4;
    }

}


else if (FIRST_AND_LAST_SECTOR[1] > 31 && (FIRST_AND_LAST_SECTOR[1] + 1) % 8 != 0)
{
    Warning_Flags += 4;
}