SPRSPB1 October 2025 F28377D-SEP
PRODUCTION DATA
The following reset sources exist on this device: XRS, WDRS, NMIWDRS, SYSRS, SCCRESET, and HIBRESET. See the Reset Signals table in the System Control chapter of the TMS320F2837xD Dual-Core Real-Time Microcontrollers Technical Reference Manual .
The parameter th(boot-mode) must account for a reset initiated from any of these sources.
Some reset sources are internally driven by the device. Some of these sources will drive XRS low. Use this to disable any other devices driving the boot pins. The SCCRESET and debugger reset sources do not drive XRS; therefore, the pins used for boot mode should not be actively driven by other devices in the system. The boot configuration has a provision for changing the boot pins in OTP; for more details, see the TMS320F2837xD Dual-Core Real-Time Microcontrollers Technical Reference Manual .