SPRSPB1 October 2025 F28377D-SEP
PRODUCTION DATA
The ADC supports two signal modes: single-ended and differential. In single-ended mode, the input voltage to the converter is sampled through a single pin (ADCINx), referenced to VREFLO. In differential signaling mode, the input voltage to the converter is sampled through a pair of input pins, one of which is the positive input (ADCINxP) and the other is the negative input (ADCINxN). The actual input voltage is the difference between the two (ADCINxP – ADCINxN). Figure 6-34 shows the differential signaling mode. Figure 6-35 shows the single-ended signaling mode.
Figure 6-34 Differential Signaling
Mode
Figure 6-35 Single-ended Signaling
Mode