SPRSPB1 October 2025 F28377D-SEP
PRODUCTION DATA
The Output X-BAR has eight outputs which can be selected on the GPIO mux as OUTPUTXBARx. The ePWM X-BAR has eight outputs which are connected to the TRIPx inputs of the ePWM. The sources for both the Output X-BAR and ePWM X-BAR are shown in Figure 5-3. For details on the Output X-BAR and ePWM X-BAR, see the Crossbar (X-BAR) chapter of the TMS320F2837xD Dual-Core Real-Time Microcontrollers Technical Reference Manual .
Figure 5-3 Output
X-BAR and ePWM X-BAR