SPRUIG1A September 2017 – October 2025
A power supply with the following specs should be used with the AM572x Evaluation Module (power supply is not included):
Figure 4-1 Isolated Power SupplyThe push button S1 near to the power cable is used for power ON/OFF. The main power is off until the push button is pressed. After pressing the S1 push button, the main power stays on for 7 seconds then powers off. To keep the power on, see the Important Notice of this document. Holding the push button for 15 seconds will forcibly turn the main power off.
Do not remove the DC power jack to turn off the board, as it may cause damage.
The proper power down procedure is documented in Important Notice of this document.
Figure 4-2 AM572x GP EVM DC Power JackThe AM572x Processor Module also includes a connector for a Lithium CR1220 non-rechargeable battery for powering a battery back external Real Time Clock (RTC) MCP79410.