SPRUIG1A September   2017  – October 2025

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4.   4
  5. Introduction
    1. 1.1 EVM System View
    2. 1.2 Schematics/Design/Errata Files
    3. 1.3 Other Useful Links
  6. Important Usage Notes
    1. 2.1 Isolated Power Supply
    2. 2.2 Powering On EVM
    3. 2.3 Powering Off EVM
    4. 2.4 Removing Processor and LCD Module Boards
    5. 2.5 Removing Camera Module Board
    6. 2.6 Caution: Hot Surface
  7. System Description
    1. 3.1 System Board Diagram
    2. 3.2 Processor
    3. 3.3 Clocks
    4. 3.4 Reset Signals
  8. Power System
    1. 4.1 Power Source
    2. 4.2 Power Nets
    3. 4.3 Power Management IC Power Supplies
    4. 4.4 APM Sense Resistors
  9. Configuration/Setup
    1. 5.1 Boot and Emulation Setup
      1. 5.1.1 Emulation and Hardware Setup
    2. 5.2 I2C Address Assignments
    3. 5.3 I2C ID Memory
  10. Processor Module Functional Block Descriptions
    1. 6.1 Memory
      1. 6.1.1 4KB EEPROM (Board Identity Memory)
      2. 6.1.2 2GB DDR3L
      3. 6.1.3 eMMC Flash Memory
      4. 6.1.4 MicroSD (MMC1) Connector
    2. 6.2 Temperature Sensor
    3. 6.3 Real Time Clock
    4. 6.4 10/100/1000 Ethernet
    5. 6.5 USB
    6. 6.6 Audio
    7. 6.7 HDMI
    8. 6.8 eSATA
    9. 6.9 Serial Debug Header
  11. AM572x EVM LCD Module Functional Block Descriptions
    1. 7.1 LCD Screen
    2. 7.2 Capacitive Touch Screen
    3. 7.3 mSATA
    4. 7.4 miniPCIe
    5. 7.5 COM8 Interface – Mobile Connectivity Expansion Connector
  12. AM572x EVM Camera Module Functional Block Descriptions
  13. Board Connectors
    1. 9.1  Gigabit Ethernet - P5 (Processor Module)
    2. 9.2  eSATA / USB - P6 (Processor Module)
    3. 9.3  USB
      1. 9.3.1 AM572x USB2 (USB 2.0 Client) - P7 (Processor Module)
      2. 9.3.2 AM572x USB1 (USB 3.0 Host) - P13, P15 (Processor Module)
    4. 9.4  Serial Debug Header - P10 (Processor Module)
    5. 9.5  HDMI - P11 (Processor Module)
    6. 9.6  MicroSD - P12 (Processor Module)
    7. 9.7  Expansion Connectors
      1. 9.7.1 Processor Module P16/LCD Module P1
      2. 9.7.2 Processor Module P17 / LCD Module P3
      3. 9.7.3 Processor Module P18 / LCD Module P4
      4. 9.7.4 Processor Module P19 / LCD Module P2
    8. 9.8  JTAG Connector
    9. 9.9  LCD Connector - P5 (LCD Module)
    10. 9.10 Touchscreen Connector - P15 (LCD Module)
    11. 9.11 PCI-Express Mini Card Slot - P7 (LCD Module)
    12. 9.12 mSATA Connector - P8 (LCD Module)
    13. 9.13 Camera Connector - P9 (LCD Module), P9 (Camera Module)
    14. 9.14 Communications Connector - P12 (LCD Module)
  14. 10References
  15. 11Revision History

eSATA

A switch is used to direct the SATA signals to the onboard eSATA connector or to the expansion header, where they are routed to the mSATA connector on the LCD Module. If the signal on the expansion header, P19-4, is left open, the signals go to the eSATA onboard connector. If the pin is grounded via the SATA_SEL jumper (J1) on the LCD Module, the switch is activated and the signals are routed to the expansion headers.

The eSATA interface on the Processor Module is a combination of two separate interfaces, SATA and USB. The eSATA port can be used as an eSATA or a USB 2.0 port. The USB signals originate from the USB 3.0 HUB. The SATA interfaces originate from the AM57xx processor via the switch.

Power for the eSATA is from the USB power pins, 5V. Power is routed to the eSATA connector via the TPS2560 FET switch. It is capable of providing the 500mA required by the eSATA connector. Only 5V is supplied.

Note:

When J1 on the LCD Module is installed (for mSATA), the eSATA on the Processor Module will no longer function. However, the connector can still function as a USB 2.0 port.