SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Table 6-2 lists the memory-mapped registers for the FLASH_CTRL_REGS registers. All register offset addresses not listed in Table 6-2 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | FRDCNTL | Flash Read Control Register | EALLOW | Go |
| 1Eh | FBAC | Flash Bank Access Control Register | EALLOW | Go |
| 20h | FBFALLBACK | Flash Bank Fallback Power Register | EALLOW | Go |
| 22h | FBPRDY | Flash Bank Pump Ready Register | EALLOW | Go |
| 24h | FPAC1 | Flash Pump Access Control Register 1 | EALLOW | Go |
| 26h | FPAC2 | Flash Pump Access Control Register 2 | EALLOW | Go |
| 2Ah | FMSTAT | Flash Module Status Register | EALLOW | Go |
| 180h | FRD_INTF_CTRL | Flash Read Interface Control Register | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 6-3 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
FRDCNTL is shown in Figure 6-4 and described in Table 6-4.
Return to the Summary Table.
Flash Read Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RWAIT | RESERVED | |||||||||||||
| R-0h | R/W-Fh | R-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-12 | RESERVED | R | 0h | Reserved |
| 11-8 | RWAIT | R/W | Fh | Random read waitstate These bits indicate how many waitstates are added to a flash read/fetch access. The RWAIT value can be set anywhere from 0 to 0xF. For a flash access, data is returned in RWAIT+1 SYSCLK cycles. Note: The required wait states for each SYSCLK frequency can be found in the device data manual. Reset type: SYSRSn |
| 7-0 | RESERVED | R | 0h | Reserved |
FBAC is shown in Figure 6-5 and described in Table 6-5.
Return to the Summary Table.
Flash Bank Access Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BAGP | RESERVED | |||||||||||||||||||||||||||||
| R-0h | R/W-0h | R/W-Fh | |||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-8 | BAGP | R/W | 0h | Bank Active Grace Period. These bits contain the starting count value for the BAGP down counter. Any access to a given bank causes its BAGP counter to reload the BAGP value for that bank. After the last access to this flash bank, the down counter delays from 0 to 255 prescaled SYSCLK clock cycles before putting the bank into one of the fallback power modes as determined by the FBFALLBACK register. This value must be greater than 1 when the fallback mode is not ACTIVE. Note: The prescaled clock used for the BAGP down counter is a clock divided by 16 from input SYSCLK. Reset type: SYSRSn |
| 7-0 | RESERVED | R/W | Fh | Reserved |
FBFALLBACK is shown in Figure 6-6 and described in Table 6-6.
Return to the Summary Table.
Flash Bank Fallback Power Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BNKPWR2 | BNKPWR1 | BNKPWR0 | ||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-6 | RESERVED | R | 0h | Reserved |
| 5-4 | BNKPWR2 | R/W | 0h | Fall Back power mode 00 Sleep (Sense amplifiers and sense reference disabled) 01 Standby (Sense amplifiers disabled, but sense reference enabled) 10 Reserved 11 Active (Both sense amplifiers and sense reference enabled) Reset type: SYSRSn |
| 3-2 | BNKPWR1 | R/W | 0h | Fall Back power mode 00 Sleep (Sense amplifiers and sense reference disabled) 01 Standby (Sense amplifiers disabled, but sense reference enabled) 10 Reserved 11 Active (Both sense amplifiers and sense reference enabled) Reset type: SYSRSn |
| 1-0 | BNKPWR0 | R/W | 0h | Fall Back power mode 00 Sleep (Sense amplifiers and sense reference disabled) 01 Standby (Sense amplifiers disabled, but sense reference enabled) 10 Reserved 11 Active (Both sense amplifiers and sense reference enabled) Reset type: SYSRSn |
FBPRDY is shown in Figure 6-7 and described in Table 6-7.
Return to the Summary Table.
Flash Bank Pump Ready Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| PUMPRDY | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BANK2RDY | BANK1RDY | BANK0RDY | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15 | PUMPRDY | R | 0h | Pump Ready. This is a read-only bit which allows software to determine if the pump is ready for flash access before attempting the actual access. If an access is made to a bank when the pump is not ready, wait states are asserted until it becomes ready. 0 Pump is not ready. 1 Pump is ready, in active power state. Reset type: SYSRSn |
| 14-3 | RESERVED | R | 0h | Reserved |
| 2 | BANK2RDY | R | 0h | Bank 2 Ready. This is a read-only register which allows software to determine if the Bank 2 is ready for Flash access before the access is attempted. Note: The user should wait for both the pump and the bank to be ready before attempting an access. 0 Bank 2 is not ready. 1 Bank 2 is in active power mode and is ready for access. Reset type: SYSRSn |
| 1 | BANK1RDY | R | 0h | Bank 1 Ready. This is a read-only register which allows software to determine if the Bank 1 is ready for Flash access before the access is attempted. Note: The user should wait for both the pump and the bank to be ready before attempting an access. 0 Bank 1 is not ready. 1 Bank 1 is in active power mode and is ready for access. Reset type: SYSRSn |
| 0 | BANK0RDY | R | 0h | Bank 0 Ready. This is a read-only register which allows software to determine if the Bank 0 is ready for Flash access before the access is attempted. Note: The user should wait for both the pump and the bank to be ready before attempting an access. 0 Bank 0 is not ready. 1 Bank 0 is in active power mode and is ready for access. Reset type: SYSRSn |
FPAC1 is shown in Figure 6-8 and described in Table 6-8.
Return to the Summary Table.
Flash Pump Access Control Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | PSLEEP | ||||||
| R-0h | R/W-A0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| PSLEEP | |||||||
| R/W-A0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PMPPWR | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-28 | RESERVED | R | 0h | Reserved |
| 27-16 | PSLEEP | R/W | A0h | Pump sleep. These bits contain the starting count value for the charge pump sleep down counter. While the charge pump is in sleep mode, the power mode management logic holds the charge pump sleep counter at this value. When the charge pump exits sleep power mode, the down counter delays from 0 to PSLEEP prescaled SYSCLK clock cycles before putting the charge pump into active power mode. Note: The pump sleep down counter uses the same prescaled clock as Bank sleep down counter which is divided by 2 of input SYSCLK. Note: BootROM configures the PSLEEP value as 0x4D4 for 120 MHz operation. Users can modify the PSLEEP value based on their application requirements if needed. Reset type: SYSRSn |
| 15-1 | RESERVED | R | 0h | Reserved |
| 0 | PMPPWR | R/W | 0h | Flash Charge Pump Fallback Power Mode. This bit selects what power mode the charge pump enters after the pump active grace period (PAGP) counter has timed out. 0 Sleep (all pump circuits disabled) 1 Active (all pump circuits active) Note for devices with multiple flash banks: As the pump is shared between flash banks, if an access is made either bank, the value of this bit changes to 1 (active). Reset type: SYSRSn |
FPAC2 is shown in Figure 6-9 and described in Table 6-9.
Return to the Summary Table.
Flash Pump Access Control Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PAGP | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | PAGP | R/W | 0h | Pump Active Grace Period. This register contains the starting count value for the PAGP mode down counter. Any access to flash memory causes the counter to reload with the PAGP value. After the last access to flash memory, the down counter delays from 0 to 65535 prescaled SYSCLK clock cycles before entering one of the charge pump fallback power modes as determined by PUMPPWR in the FPAC1 register. Note: The PAGP down counter is clocked by the same prescaled clock as the BAGP down counter which is divided by 16 of input SYSCLK. Reset type: SYSRSn |
FMSTAT is shown in Figure 6-10 and described in Table 6-10.
Return to the Summary Table.
Flash Module Status Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RESERVED | RESERVED | |||||
| R-0h | R-0h | R-0h | |||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RESERVED | RESERVED | PGV | RESERVED | EV | RESERVED | BUSY |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ERS | PGM | INVDAT | CSTAT | VOLTSTAT | ESUSP | PSUSP | RESERVED |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-18 | RESERVED | R | 0h | Reserved |
| 17 | RESERVED | R | 0h | Reserved |
| 16 | RESERVED | R | 0h | Reserved |
| 15 | RESERVED | R | 0h | Reserved |
| 14 | RESERVED | R | 0h | Reserved |
| 13 | RESERVED | R | 0h | Reserved |
| 12 | PGV | R | 0h | Program verify When set, indicates that a word is not successfully programmed after the maximum allowed number of program pulses are given for program operation. Reset type: SYSRSn |
| 11 | RESERVED | R | 0h | Reserved |
| 10 | EV | R | 0h | Erase verify When set, indicates that a sector is not successfully erased after the maximum allowed number of erase pulses are given for erase operation. Reset type: SYSRSn |
| 9 | RESERVED | R | 0h | Reserved |
| 8 | BUSY | R | 0h | When set, this bit indicates that a program, erase, or suspend operation is being processed. Reset type: SYSRSn |
| 7 | ERS | R | 0h | Erase Active. When set, this bit indicates that the flash module is actively performing an erase operation. This bit is set when erasing starts and is cleared when erasing is complete. It is also cleared when the erase is suspended and set when the erase resumes. Reset type: SYSRSn |
| 6 | PGM | R | 0h | Program Active. When set, this bit indicates that the flash module is currently performing a program operation. This bit is set when programming starts and is cleared when programming is complete. It is also cleared when programming is suspended and set when programming is resumed. Reset type: SYSRSn |
| 5 | INVDAT | R | 0h | Invalid Data. When set, this bit indicates that the user attempted to program a '1' where a '0' was already present. Reset type: SYSRSn |
| 4 | CSTAT | R | 0h | Command Status. Once the FSM starts any failure will set this bit. When set, this bit informs the host that the program, erase, or validate sector command failed and the command was stopped. This bit is cleared by the Clear Status command. For some errors, this will be the only indication of an FSM error because the cause does not fall within the other error bit types. Reset type: SYSRSn |
| 3 | VOLTSTAT | R | 0h | Core Voltage Status. When set, this bit indicates that the core voltage generator of the pump power upply dipped below the lower limit allowable during a program or erase operation. Reset type: SYSRSn |
| 2 | ESUSP | R | 0h | When set, this bit indicates that the flash module has received and processed an erase suspend operation. This bit remains set until the erase resume command has been issued or until the Clear_More command is run. Reset type: SYSRSn |
| 1 | PSUSP | R | 0h | When set, this bit indicates that the flash module has received and processed a program suspend operation. This bit remains set until the program resume command has been issued or until the Clear_More command is run. Reset type: SYSRSn |
| 0 | RESERVED | R | 0h | Reserved |
FRD_INTF_CTRL is shown in Figure 6-11 and described in Table 6-11.
Return to the Summary Table.
Flash Read Interface Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DATA_CACHE_EN | PREFETCH_EN | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-2 | RESERVED | R | 0h | Reserved |
| 1 | DATA_CACHE_EN | R/W | 0h | Data cache enable. 0 A value of 0 disables the data cache. 1 A value of 1 enables the data cache. Reset type: SYSRSn |
| 0 | PREFETCH_EN | R/W | 0h | Prefetch enable. 0 A value of 0 disables prefetch mechanism. 1 A value of 1 enables pre-fetch mechanism. Reset type: SYSRSn |