SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
FILE: fsi_ex1_loopback_cpucontrol.c
Example sets up infinite data frame transfers where trigger happens through CPU. Automatic(Hw triggered) Ping frame transmission is also setup along with data.
User can edit some of configuration parameters as per usecase. These are as below. Default values can be referred in code where these globals are defined
External Connections
For FSI internal loopback (EXTERNAL_FSI_ENABLE == 0), no external connections needed
For FSI external loopback (EXTERNAL_FSI_ENABLE == 1), external connections are required. The FSI TX pins should be connected to the FSI RX pins of the same device. See below for external connections to include and GPIOs used:
External Connections Required between FSI TX and RX of the same device:
ControlCard FSI Header GPIOs:
Watch Variables