SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The timer can be configured to provide a programmable PWM output. The timer PWM (POTIMERPWM) output pin can be configured to toggle on an event. The TIMER_TCLR[11-10] TRG bit field determines on which register value the PWM pin toggles. Either overflow or both overflow and match can be selected to toggle the timer PWM pin when a compare condition occurs.
In toggle mode, when TIMER_TCLR[11-10] TRG = 0x2 (overflow and match), the first event that toggles the PWM line is an overflow event.
The TIMER_TCLR[7] SCPWM bit can be programmed to set or clear the timer PWM output signal only while the counter is stopped or the trigger is off. This allows setting the output pin to a known state before modulation starts. Modulation synchronously stops when the TIMER_TCLR[11-10] TRG bit field is cleared and overflow occurs. This allows fixing a deterministic state of the output pin when modulation stops.
In Figure 12-464, the internal overflow pulse is set each time the (0xFFFF FFFF – TIMER_TLDR[31-0] LOAD_VALUE + 1) value is reached, and the internal match pulse is set when the counter reaches the value of TIMER_TMAR. Depending on the value of the TIMER_TCLR[12] PT bit and TIMER_TCLR[11-10] TRG bit field, the timer provides pulse or PWM event on the output pin (POTIMERPWM).
The TIMER_TLDR and TIMER_TMAR must keep values below the overflow value (0xFFFF FFFF) by at least two units. If the PWM trigger events are both overflow and match, the difference between the values kept in the TIMER_TMAR and the value in the TIMER_TLDR must be at least two units. When match event is used, the compare mode TIMER_TCLR[6] CE bit must be set.
In Figure 12-464, the TIMER_TCLR[7] SCPWM bit is set to 0. In Figure 12-465, the TIMER_TCLR[7] SCPWM bit is set to 1. To obtain the desired wave form, start the counter at 0xFFFF FFFE value (to ensure an overflow first) or adjust the line polarity (TIMER_TCLR[7] SCPWM bit).