SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The histogram can work on either one of the color components after the CCM-1 or the fourth color component routed directly from the Flexible CFA. The Histogram can also work on internally generated Luma value using simple averaging of RGB components. The Histogram module supports a local memory which can be read by the host processor. The Histogram provides data which can be used by the software to generate tone curves for the Contrast Stretch LUT.
The input to the Histogram module is calculated based on the control MMR as it follows:
The histogram module downsamples the image in the horizontal direction by a factor of 2 using simple averaging filter. This ensures that the memory access requirements of the module are limited to 1 read + 1 write access every 2 cycles (1 access/cycle) and thus can be achieved using a simple memory architecture.
The histogram module requires a ping-pong memory which is mapped to the configuration bus. This allows for histogram operation to run in concurrent with the Read operation from the host. For ease of software complexity, both the Ping/Pong memories map to the same address and it is the responsibility of the design to ensure that the muxing logic always take care of the correct access from both the host and the module. To detect error conditions, if the host is not able to read fast enough from the memory, an error interrupt should be generated whenever the host has initiated a read transfer from the first location of the memory but has not initiated a read transfer from the last location of the memory.
The Histogram module has 2 banks of memores each of 256x20 bits which are used in ping pong fashion. The input pixel has to be downshifted to match the bin size. The Histogram module has separate registers for creating an ROI using horizontal/vertical start postions as well as horizontal/vertical size.
Typically the ROI registers (VISS_FCP_FCC_CFG_HIST_1 and VISS_FCP_FCC_CFG_HIST_2) have to be set that at least one line is skipped for histogram calculation. The one line of time can be used by the histogram module to set the value of each of the bins to zero. This also puts a constraint on the histogram ROI to have a minmum width of 256 pixels.