SPRUJ69 December 2022 TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The EVM provides several expansion interfaces that have non-standard/custom pinouts. Each of these interfaces are introduced and specific pin information is provided.
Note: that some of the interfaces include ‘Direction’ information. This is relative to the EVM, so INPUT is input to the EVM/output of the connected device. OUTPUT is output of the EVM/input to the connected device.