SPRUJ69 December 2022 TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Five UART ports of the processor are interfaced with the UART-over-USB transceiver(s). When the EVM’sUSB micro-B connectors [J43] and/or [J44] are connected to a Host-PC using supplied USB cable (Type-A to Micro-B), the computer can establish Virtual Com Port(s) to be used with any terminal application. Virtual Com Port drivers for the transceiver(s) can be obtained from:
https://www.ftdichip.com/Products/ICs/FT2232H.html
https://www.ftdichip.com/Products/ICs/FT4232H.html
Once installed, the Host-PC will create the Virtual Com Ports (two ports for FT2232, 4 ports for FT4232). Depending on the other Host-PC resources available, the Com Ports may not be located at COM1-2 and/or COM1-4. However, they will remain in the same numerical order for each transceiver.
The circuit(s) are powered from USB bus power and therefore the COM connection will not be lost when the EVM power is removed. LED(s) [LD11] [LD10] are used to indicate an active COM connection with Host-PC.
UART Port | Host-PC COM Port |
---|---|
MCU_UART0 | COM 1 |
WKUP_UART0 | COM 2 |
UART Port | Host-PC COM Port |
---|---|
MAIN_UART8 | COM 1 |
MAIN_UART5 | COM 2 |
MAIN_UART2 | COM 3 |
NA | COM 4 |
The EEPROM of FTDI bridges are programmed with the CPB serial number, users to identify the connected COM port with board serial number when one or more boards connected to the computer.