SPRUJC9B March 2025 – January 2026 AM62L
When selecting crystal for WKUP_OSC0 or LFOSC0, the recommendation is to consider the temperature and aging characteristics based on the worst case operating environment and expected life expectancy of the custom board or the end equipment. Verify the crystal load and the crystal load capacitor value used (including addition of the PCB capacitance (for WKUP_OSC0)) matches the device-specific data sheet recommendations. The recommendation is to select crystal load which allows selection of a standard capacitor value. Mismatch in value can introduce clock frequency PPM errors.
For more information, see the following FAQ:
For more information, see the WKUP_OSC0 Crystal Circuit Requirements and LFOSC0 Crystal Electrical Characteristics tables of the device-specific data sheet.
The recommendation is to connect the WKUP_OSC0 crystal directly to the processor as per device-specific data sheet.
The recommendation is to verify the crystal selection with the crystal manufacturer (as required).