SPRUJC9B March 2025 – January 2026 AM62L
The processor family supports pinouts (pin attributes defined) for DPI and DSI interfaces. The processor (internal hardware) supports configuring (using) either MIPI DSI (x4 lanes D-PHY (DPHY)) or DPI (24-bit RGB LVCMOS) display (external). The selection of the processor display interface is required to be done at boot time.
MIPI Display Serial Interface (DSI) D-PHY (DPHY) display interface:
The processor family supports DSI with x4 (four) data lanes and x1 (single) clock lane. For connecting DSITX0 signals when not used (complete or partial), see the Pin Connectivity Requirements section of the device-specific data sheet.
DPI (Display Parallel Interface):
The processor family supports 24-bit per pixel, RGB/YUV422 modes, LVCMOS output, DPI (parallel) display interface.
Spread Spectrum clocking for Display Parallel Interface (DPI) is currently supported. For more information, refer AM62x, AM62Ax, AM62Px, AM62Lx Spread-Spectrum Clocking application note.
Processor IO buffers are off during reset and after reset. Parallel pulls are recommended for any of the processor IOs (DPI interface signals) that can float (to prevent the attached device inputs from floating until driven by the host).
For more information on DPI, see the following FAQ:
The FAQ is generic and can also be used for AM62Lx processor family.
For more information, see the Display Subsystem and Peripherals section in the Peripherals chapter of the device-specific TRM.