SPRZ575A March   2024  – April 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1

 

  1.   1
  2. 1Modules Affected
  3. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development-Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  4. 3Silicon Revision 1.0 Usage Notes and Advisories
    1. 3.1 Silicon Revision 1.0 Usage Notes
      1.      i2134
    2. 3.2 Silicon Revision 1.0 Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2120
      5.      i2137
      6.      i2160
      7.      i2189
      8.      i2190
      9.      i2196
      10.      i2199
      11.      i2208
      12.      i2242
      13.      i2243
      14.      i2249
      15.      i2253
      16.      i2278
      17.      i2279
      18.      i2310
      19.      i2311
      20.      i2312
      21.      i2326
      22.      i2330
      23.      i2351
      24.      i2362
      25.      i2366
      26.      i2372
      27.      i2383
      28.      i2399
      29.      i2401
      30.      i2407
      31.      i2409
      32.      i2410
      33.      i2419
      34.      i2424
      35.      i2431
      36.      i2436
      37.      i2457
      38.      i2478
  5.   Trademarks
  6. 4Revision History

Modules Affected

Table 1-1 shows the module(s) that are affected by each usage note.

Table 1-1 Usage Note by Modules
MODULE USAGE NOTE
USB i2134 — USB: 2.0 Compliance Receive Sensitivity Test Limitation

Table 1-2 shows the module(s) that are affected by each advisory.

Table 1-2 Advisories by Modules
MODULE ADVISORY
BCDMA i2431 — BCDMA: RX Channel can lockup in certain scenarios
i2436 — BCDMA: BCDMA RX_IGNORE_LONG setting in RX CHAN CFG register doesn't work
Boot i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation
i2372 — Boot: ROM doesn't support select multi-plane addressing schemes in Serial NAND boot
i2410 — Boot: ROM may fail to boot due to i2409
i2419 — Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled
i2457 — Boot: Missing data in UART transfer causes boot failures
C7x SE i2120 — C71x: SE Hangs on Non-Parity Error Detection in Transposed Streams With LEZR
i2199 — C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary
i2399 — C7x: CPU NLC Module Not Clearing State on Interrupt
CPSW i2208 — CPSW: ALE IET Express Packet Drops
i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up
CSI i2190 — CSI_RX_IF may enter unknown state following an incomplete frame
DDR i2160 — DDR: Valid VRef Range Must be Defined During LPDDR4 Command Bus Training
i2330 — DDRSS Register Configuration Tool Updates
DSS i2097 — DSS: Disabling a Layer Connected to Overlay May Result in Synclost During the Next Frame
ECC AGGR i2049 — ECC AGGR: Potential IP Clockstop/reset sequence hang due to pending ECC Aggregator interrupts
IA i2196 — IA: Potential deadlock scenarios in IA
MCAN i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID
i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID
MMCSD i2312 — MMCSD: HS200 and SDR104 Command Timeout Window Too Small
i2478 — MMCSD0: HS400 Mode not supported
OSPI i2189 — OSPI: Controller PHY Tuning Algorithm
i2249 — OSPI: Internal PHY Loopback and Internal Pad Loopback clocking modes with DDR timing inoperable
i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash
i2383 — OSPI: 2-byte address is not supported in PHY DDR mode
PCIe i2242 — PCIe: The SerDes PCIe Reference Clock Output is temporarily disabled while changing Data Rates
i2243 — PCIe: Timing requirement for disabling output refclk during L1.2 substate is not met
i2326 — PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limits
PLL i2424 — PLL: PLL Programming Sequence May Introduce PLL Instability
PRG i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure
PSIL i2137 — Clock stop operation can result in undefined behavior
RAT i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set
Reset i2407 — RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted low
SGMII i2362 — 10-100M SGMII: Marvell PHY does not ignore the preamble byte resulting in link failure
USART i2310 — USART: Erroneous clear/trigger of timeout interrupt
i2311 — USART: Spurious DMA Interrupts
USB i2409 — USB2 PHY locks up due to short suspend