SWRA826 August   2025 CC1312R7 , CC1314R10 , CC1352P7 , CC1354P10 , CC1354R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Acronyms
  5. Introduction
  6. Network Configuration
  7. Wi-SUN FAN and Joining Process
    1. 4.1 Wi-SUN FAN
    2. 4.2 Joining Process
  8. Test Results
    1. 5.1 Join Time - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    2. 5.2 Rejoin Time - One Router Node
    3. 5.3 Rejoin Time - Full Network
    4. 5.4 Throughput - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    5. 5.5 BR Detection of RN Disconnection
    6. 5.6 RN Detection of BR Disconnection
  9. Latency
  10. Preferred Parent and Disconnected Parent
    1. 7.1 Preferred Parent
    2. 7.2 Disconnected Parent
    3. 7.3 Test Results for Preferred Parent and Disconnected Parent
  11. Additional Information
  12. Summary
  13. 10References

Rejoin Time - Full Network

Similar to the 1RN Rejoin time, the full network rejoin time measures the time for every router node to reconnect back to the border router device. This test is used to simulate a full power down scenario in the field, allowing estimation of the performance in an area where there is an elevated risk of the router nodes losing power. The full network rejoin test uses the same topology as the initial join time tests to avoid any possible changes due to a different network topology. Figure 5-7 shows a diagram of the full network rejoin test. All router nodes are reset and the time to rejoin the network is measured.

 Full Network Rejoin Time Test
                    Setup Figure 5-7 Full Network Rejoin Time Test Setup

Figure 5-8 and Figure 5-9 show the rejoin time results using the setup above. The test is run using both a 50kbps and a 300kbps PHY.

 Full Network Rejoin Time for
                    Maximize Responsiveness, Balanced Mode, Maximize Scalability Network
                    Configurations (50kbps PHY) Figure 5-8 Full Network Rejoin Time for Maximize Responsiveness, Balanced Mode, Maximize Scalability Network Configurations (50kbps PHY)
 Full Network Rejoin Time for
                    Maximize Responsiveness, Balanced Mode, Maximize Scalability Network
                    Configurations (300kbps PHY) Figure 5-9 Full Network Rejoin Time for Maximize Responsiveness, Balanced Mode, Maximize Scalability Network Configurations (300kbps PHY)

Since the router nodes have already been configured during the initial join, the router nodes can retain the configuration and GTKs which makes the rejoin time faster than the initial join time. For maximize responsiveness and balanced mode configurations, the PHY does not make a big difference as the determining factor is still the protocol timers. However, at maximize scalability, since the protocol overhead is low, the protocol timers are no longer the only determining factor and increased data rate provides a noticeable improvement in rejoin time.