SWRA826 August   2025 CC1312R7 , CC1314R10 , CC1352P7 , CC1354P10 , CC1354R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Acronyms
  5. 2 Introduction
  6. 3 Network Configuration
  7. 4 Wi-SUN FAN and Joining Process
    1. 4.1 Wi-SUN FAN
    2. 4.2 Joining Process
  8. 5 Test Results
    1. 5.1 Join Time - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    2. 5.2 Rejoin Time - One Router Node
    3. 5.3 Rejoin Time - Full Network
    4. 5.4 Throughput - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    5. 5.5 BR Detection of RN Disconnection
    6. 5.6 RN Detection of BR Disconnection
  9. 6 Latency
  10. 7 Preferred Parent and Disconnected Parent
    1. 7.1 Preferred Parent
    2. 7.2 Disconnected Parent
    3. 7.3 Test Results for Preferred Parent and Disconnected Parent
  11. 8 Additional Information
  12. 9 Summary
  13. 10References

Join Time - Maximize Responsiveness, Balanced Mode, Maximize Scalability

Join time is the time required for all router nodes to join a new network. The test is carried out using the setup shown in Figure 5-2 for each network configuration. Figure 5-3 plots the number of nodes joined in the network versus the time required to do so.

 Large Network Test
                    Setup Figure 5-2 Large Network Test Setup
 Wi-SUN® Join Time for Maximize
                    Responsiveness, Balanced Mode, Maximize Scalability Network Configurations
                    (50kbps PHY) Figure 5-3 Wi-SUN® Join Time for Maximize Responsiveness, Balanced Mode, Maximize Scalability Network Configurations (50kbps PHY)
 Wi-SUN® Join Time for Maximize
                    Responsiveness, Balanced Mode, Maximize Scalability Network Configurations
                    (300kbps PHY) Figure 5-4 Wi-SUN® Join Time for Maximize Responsiveness, Balanced Mode, Maximize Scalability Network Configurations (300kbps PHY)

The maximize responsiveness network configuration connects the fastest, which is the expected result based on the definition for each of the configurations in Section 3.

While 300kbps has a lower join time due to higher data rate, this does not provide a significant or proportional reduction. This is expected as the determining factor for the join time are the protocol timer configurations at different layers of the protocol stack.