SWRA826 August   2025 CC1312R7 , CC1314R10 , CC1352P7 , CC1354P10 , CC1354R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Acronyms
  5. Introduction
  6. Network Configuration
  7. Wi-SUN FAN and Joining Process
    1. 4.1 Wi-SUN FAN
    2. 4.2 Joining Process
  8. Test Results
    1. 5.1 Join Time - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    2. 5.2 Rejoin Time - One Router Node
    3. 5.3 Rejoin Time - Full Network
    4. 5.4 Throughput - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    5. 5.5 BR Detection of RN Disconnection
    6. 5.6 RN Detection of BR Disconnection
  9. Latency
  10. Preferred Parent and Disconnected Parent
    1. 7.1 Preferred Parent
    2. 7.2 Disconnected Parent
    3. 7.3 Test Results for Preferred Parent and Disconnected Parent
  11. Additional Information
  12. Summary
  13. 10References

Rejoin Time - One Router Node

During operation, disconnect a router node from the network. One router node rejoin time measures the time required for the router node to reconnect back to the PAN. The measurement is done by disconnecting a device in a fully joined network (see Figure 5-5) and is carried over in each network configuration (maximize responsiveness, balanced mode, maximize scalability).

 One Router Node Rejoin Time
                    Test Diagram  One Router Node Rejoin Time
                    Test Diagram Figure 5-5 One Router Node Rejoin Time Test Diagram
 One Router Node Rejoin Time
                    for Maximize Responsiveness, Balanced Mode, Maximize Scalability Network
                    Configurations Figure 5-6 One Router Node Rejoin Time for Maximize Responsiveness, Balanced Mode, Maximize Scalability Network Configurations

Similar to the join time results, the maximize responsiveness network rejoins the fastest due to the increased number of messages exchanged between the RNs and the BR over a period of time.