SWRA826 August 2025 CC1312R7 , CC1314R10 , CC1352P7 , CC1354P10 , CC1354R10
Table 7-1 shows the recorded times for preferred parent and ran over five separate tests, where the RN had to change the preferred parent. The average time is shown in the last row of Table 7-1.
| Test # | Time (sec) |
|---|---|
| 1 | 46 |
| 2 | 36 |
| 3 | 41 |
| 4 | 66 |
| 5 | 51 |
| Average | 48 |
During the preferred parent test, the router nodes usually undergo reconfiguration in less than one minute.
Similar to the preferred parent tests, Table 7-2 shows the recorded times for the five separate disconnected parent tests, where the RN had to change the parent due to a disconnection of a previous RN in the chain. The average time is shown in the last row of Table 7-2.
| Run # | Time (sec) |
|---|---|
| 1 | 73 |
| 2 | 156 |
| 3 | 110 |
| 4 | 141 |
| 5 | 108 |
| Average | 117 |
The disconnected parent example shows that the router nodes generally take less than 2 minutes to notice a broken link to the BR and reconfigure themselves accordingly. Note, however, that the border router disconnection time is 30 seconds, bringing the disconnected parent detection time down to 87s.