SWRA826 August   2025 CC1312R7 , CC1314R10 , CC1352P7 , CC1354P10 , CC1354R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Acronyms
  5. 2 Introduction
  6. 3 Network Configuration
  7. 4 Wi-SUN FAN and Joining Process
    1. 4.1 Wi-SUN FAN
    2. 4.2 Joining Process
  8. 5 Test Results
    1. 5.1 Join Time - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    2. 5.2 Rejoin Time - One Router Node
    3. 5.3 Rejoin Time - Full Network
    4. 5.4 Throughput - Maximize Responsiveness, Balanced Mode, Maximize Scalability
    5. 5.5 BR Detection of RN Disconnection
    6. 5.6 RN Detection of BR Disconnection
  9. 6 Latency
  10. 7 Preferred Parent and Disconnected Parent
    1. 7.1 Preferred Parent
    2. 7.2 Disconnected Parent
    3. 7.3 Test Results for Preferred Parent and Disconnected Parent
  11. 8 Additional Information
  12. 9 Summary
  13. 10References

Disconnected Parent

The same configuration, as shown in Section 7.1, can be used to give an overview of the disconnected parent case (see Figure 7-4).

 Disconnected Parent Example:
                    Initial Setup Figure 7-4 Disconnected Parent Example: Initial Setup

In this scenario, Router Node 1 is disconnected, severing communication between the Border Router and Router Nodes 2 and 3, as shown in Figure 7-5.

 Disconnected Parent Example:
                    Disconnect RN1 Figure 7-5 Disconnected Parent Example: Disconnect RN1

When the disconnection of the parent router node is detected by Router Node 2, Router Node 2 tries to connect to the closest available alternative (see Figure 7-6). This is Router Node 4 in this scenario

 Disconnected Parent Example:
                    Observe Rerouting across RN4 Figure 7-6 Disconnected Parent Example: Observe Rerouting across RN4