SWRU633 September 2026
An LP-XDS110 or LP-XDS110ET is used to interface between SmartRF Studio 8 and the CC1407P device on the BoosterPack through the 20-pin edge connector. To use the BoosterPack with SmartRF Studio 8, simply connect the 20-pin edge connector to the XDS debugger as shown in Figure 2-3 and connect the XDS debugger to a computer with a USB cable.