TIDUD61E October 2020 – April 2021
The DC bus regulation loop is assumed to provide the power reference. The power reference is then divided by the square of the line voltages RMS to provide the conductance, which is further multiplied by the line voltage giving the instantaneous current command.
Small signal model of the DC bus regulation loop is developed by linearizing Equation 4 around the operating point.
For a resistive load the bus voltage and current are related as shown in Equation 5.
The DC voltage regulation loop control model can be drawn as shown in Figure 2-11. An additional Vbus feedforward is applied to make the control loop independent of the bus voltage, and hence, the plant model for the bus control can be written as Equation 6.

Figure 2-11
DC Voltage Loop Control ModelUsing Figure 2-11, a proportional integrator (PI) compensator is designed for the voltage loop. The bandwidth of this loop is kept low as it is in conflict with the THD under steady state.
SFRA library is used to measure the frequency response on the voltage loop and verify the model. Figure 2-12 shows the modelled versus measured plots for the voltage loop.
Figure 2-12 Gv, Voltage Loop Modeled Versus Measured