TIDUD61E October 2020 – April 2021
In this build, Lab 2, the inner current loop is closed that is the inductor current is controlled using a current compensator Gi. Both DC bus and output voltage feed forward are applied to the output of this current compensator to generate the duty cycle of the inverter, Equation 7. This makes the plant for the current compensator simple and a proportional (P) controller can be used to tune the loop of the inner current. The model for the current loop was derived in section Section 2.4.2. Complete software diagram for this build is illustrated in Figure 3-13.
Complete software diagram for this lab as illustrated in Figure 3-13.
Figure 3-13 Lab 2 Control Software Diagram: Closed Current
Loop