TIDUD61E October 2020 – April 2021
Most power electronics converters require protection from overcurrent event. For this design multiple comparators are required, and references for the trip must be generated, as shown in Figure 2-6.
Figure 2-6 Trip Generation for PWM Using Comparators and Reference GeneratorsAll this circuitry is avoided when using C2000 MCUs, such as TMS320F28377D, which have on-chip windowed comparator as part of the CMPSS that are internally connected to the PWM module that can enable fast tripping of the PWM. An on-chip windowed comparator saves board space and cost in the end application as extra components can be avoided using on-chip resources, as shown in Figure 2-7.
Figure 2-7 CMPSS Used for Overcurrent Protection