TIDUEO0C July 2019 – March 2021
Figure 2-6 shows the TINA-TI simulation results with the current flowing through the 0.1-Ω resistance. When injecting a 493-mA current into the system, the input voltage of operational amplifier is 69.03 mV (slightly above the calculated 69 mV). The resulting output voltage is 3.29 V, which is close to the calculations in Section 2.4.2.2 and the 3.3 V full-scale voltage.
Figure 2-6 TINA-TI Simulation for the High-Current Range Using 0.1-Ω Resistor ValueFigure 2-7 shows the simulation of the current flowing through the 6.8-kΩ resistor. With 10-µA current into the system, the input voltage of the LPV521 device is 67.99 mV (a bit below the 69 mV maximum value).
Figure 2-7 TINA-TI Simulation for the Low-Current Range Using 6.8-kΩ Resistor ValueThe simulated output voltage is 3.24 V, also slightly below the maximum allowed voltage of 3.3 V, which is in line with the calculated results.
Using the TINA-TI simulation file included with this reference design, designers can calculate the resistor values required for their application.