For this design, the following general guidelines
must be followed:
- Place decoupling capacitors close to the
associated pins of the capacitors.
- Use ground planes instead of ground traces and
minimize the cuts in the ground plane, especially
near the ADS131M08. In this design, there is a
ground plane on both the top and bottom layer; for
this situation, make sure that there is good
stitching between the planes through the liberal
use of vias.
- Keep the two traces to the inputs of an ADC
channel symmetrical and as close as possible to
each other.
- Crosstalk from the voltage to current channels
can reduce accuracy at lower currents if power
offset is not performed. To minimize voltage to
current crosstalk on the PCB, assign ADC channels
0, 1, and 2 to the current channels and channels
3, 4, and 5 to the voltage channels or vice versa:
ADC channels 0, 1, and 2 are the voltage channels
and channels 3, 4, and 5 are the current
channels.
- For the ADS131M08 device, place the 0.1μF
capacitor closest to the AVDD pin than the 1μF
capacitor. Do the same thing also for the 0.1μF
and 1μF capacitors connected to DVDD.
- The order of the AINxP and AINxN pins on the ADS131M08 switches when going from
one converter channel to another. This swapped order is dealt with in this
design by routing the connections at J4 and J6 on the PCB accordingly.
- Minimize the length of the traces used to connect
the crystal to the microcontroller. Place guard
rings around the leads of the crystal and ground
the crystal housing. In addition, there must be
clean ground underneath the 16.384MHz crystal and
placing any traces underneath the crystal must be
avoided. Also, keep high-frequency signals away
from the crystal.
- Use wide traces for power-supply
connections.
- Use a different ground plane for the isolated
RS-232 and RS-485. This other ground plane is at
the potential of the RS-232 and RS-485 ground and
not the GND used elsewhere in the board.
- Make sure that the recommended clearance and
creepage spacing are met for the ISO6731 and
ISO6720 isolation devices in this design.