The design has support for 3-phase +
Neutral configuration with current transformers (CT). AC voltages and currents can
be applied to the board for testing purposes at these points:
- Terminal blocks J1, J2, and J3, correspond
to the line voltage connections for Phases A, B, and C, respectively. These
terminal blocks have two positions.
- Terminal blocks J4, J5, and J6 correspond to
the current inputs after the sensors for Phases A, B, and C, respectively.
These are three-position terminal blocks but only the leftmost and rightmost
positions are used. The center position, which is connected to GND, is not
connected to the CT. Select the applied current to the input of the CT so
that the current does not exceed 100A. In addition, before performing any
test, verify that this terminal block is securely connected to both
output leads of the CT.
- Terminal block J15 corresponds to the current input after
the sensor for the Neutral line. This terminal block is a three-position
terminal block but only the leftmost and rightmost positions are used. The
center position, which is connected to GND, is not connected to the CT.
Select the applied current to the input of the CT so that the current does
not exceed 100A. In addition, before performing any test, verify that
this terminal block is securely connected to both output leads of the
CT.
Figure 4-2 and
Figure 4-3
show the various test setup connections required for the reference design to
function properly for the one-voltage configuration.
Figure 4-2 Test Setup
Configuration