TIDUF25A June 2023 – March 2025 ADS131M08 , MSPM0G1507
For the following test results, gain and phase calibration are applied to the meter. In the following results, the active energy results are within 0.1% at 0° phase shift. Additionally, the active energy versus voltage results and the RMS voltage results show that good accuracy results are able to be obtained despite using only a fraction of the ADC range for the voltage channels.
The "% Error" columns in the following 6 tables and plots are calculated as the difference between the multiple reference input values to TIDA-010243 and the measured values, shown on the PC GUI. The reference input values to TIDA-010243 are generated by a PTS3.3C Source Generator/Reference Meter from the company MTE, while the measured values calculated by the TIDA-010243 Energy Library are reported in the PC GUI.
| VOLTAGE (V) | % ERROR |
|---|---|
| 270 | 0.00555 |
| 260 | 0.00384 |
| 240 | 0.00375 |
| 230 | 0.01086 |
| 220 | 0.00863 |
| 200 | 0.00700 |
| 180 | 0.01055 |
| 160 | 0.00250 |
| 140 | 0.00214 |
| 120 | 0.00666 |
| 100 | 0.00300 |
| 90 | 0.01300 |
| 70 | 0.01571 |
| 50 | 0.00240 |
| 30 | 0.01200 |
| 10 | 0.00299 |
| 9 | 0.02733 |
| CURRENT (A) | % ERROR |
|---|---|
0.01 |
0.50383 |
0.03 |
0.20413 |
| 0.05 | 0.07749 |
0.1 |
0.00399 |
0.25 |
0.02239 |
0.50 |
0.00179 |
1.00 |
0.01999 |
2.00 |
0.01649 |
5.00 |
0.00539 |
10.00 |
0.00999 |
20.00 |
0.01449 |
| 30.00 | 0.03366 |
40.00 |
0.01124 |
| 50.00 | 0.01398 |
| 60.00 | 0.01566 |
70.00 |
0.00642 |
| 80.00 | 0.00749 |
| 90.00 | 0.02321 |
100.00 |
0.02099 |
| VOLTAGE (V) | % ERROR |
|---|---|
270 |
0.01444 |
260 |
0.01307 |
| 240 | 0.00500 |
230 |
0.00304 |
220 |
0.01090 |
200 |
0.00500 |
180 |
0.00111 |
160 |
0.00687 |
140 |
0.00428 |
| 120 | 0.01916 |
100 |
0.00900 |
90 |
0.00922 |
70 |
0.02771 |
| 50 | 0.02240 |
| 30 | 0.02500 |
| 10 | 0.03400 |
9 |
0.02133 |
| CURRENT (A) | % ERROR |
|---|---|
0.01 |
0.63311 |
0.03 |
0.26816 |
| 0.05 | 0.07893 |
0.10 |
0.04498 |
| 0.25 | 0.01159 |
| 0.50 | 0.01220 |
| 1.00 | 0.01499 |
| 2.00 | 0.00449 |
| 5.00 | 0.01339 |
| 10.00 | 0.00100 |
| 20.00 | 0.01449 |
| 30.00 | 0.02666 |
| 40.00 | 0.02825 |
| 50.00 | 0.01019 |
| 60.00 | 0.01683 |
| 70.00 | 0.00414 |
| 80.00. | 0.00475 |
| 90.00 | 0.01988 |
| 100.00 | 0.03199 |
| VOLTAGE (V) | % ERROR |
|---|---|
| 9 | 0.02077 |
| 10 | 0.00699 |
| 30 | 0.00566 |
| 50 | 0.00960 |
| 70 | 0.00528 |
| 90 | 0.00988 |
| 100 | 0.00200 |
| 120 | 0.00999 |
| 140 | 0.00071 |
| 160 | 0.01874 |
| 180 | 0.00388 |
| 200 | 0.00650 |
| 220 | 0.00090 |
| 230 | 0.01652 |
| 240. | 0.01124 |
| 260 | 0.02461 |
| 270 | 0.02444 |
| CURRENT (A) | % ERROR |
|---|---|
| 0.01 | 0.32617 |
0.03 |
0.15916 |
| 0.05 | 0.09126 |
0.10 |
0.00499 |
| 0.25 | 0.00200 |
| 0.50 | 0.01940 |
| 1.00 | 0.00500 |
| 2.00 | 0.00699 |
| 5.00 | 0.01139 |
| 10.00 | 0.09506 |
| 20.00 | 0.05700 |
| 30.00 | 0.02899 |
| 40.00 | 0.03625 |
| 50.00 | 0.01720 |
| 60.00 | 0.01166 |
| 70.00 | 0.01842 |
| 80.00. | 0.01062 |
| 90.00 | 0.00100 |
| 100.00 | 0.00120 |
| CURRENT (A) | AVG ERROR % PF = 1, cos ϕ = 0° | LIMIT (%) [CLASS 0.2] IEC 62053-22 (PF 0.5i/0.8c) | LIMIT (%) [CLASS 0.5] IEC 62053-22 (PF 0.5i/0.8c) | AVG ERROR % PF = 0.5i, cos ϕ = 60° | LIMIT (%) [CLASS 0.2] IEC 62053-22 (PF 0.5i/0.8c) | LIMIT (%) [CLASS 0.5] IEC 62053-22 (PF 0.5i/0.8c) | AVG ERROR % PF = 0.8c, cos ϕ = –36.87° |
|---|---|---|---|---|---|---|---|
| 0,1 | 0,026 | 0,4 | 1,0 | –0,002 | 0,5 | 1,0 | 0,038 |
| 0,5 | 0,021 | 0,4 | 1,0 | –0,013 | 0,5 | 1,0 | 0,035 |
| 0,75 | 0,023 | 0,4 | 1,0 | –0,004 | 0,5 | 1,0 | 0,037 |
| 1,5 | 0,017 | 0,2 | 0,5 | –0,011 | 0,3 | 0,6 | 0,029 |
| 3 | 0,022 | 0,2 | 0,5 | –0,012 | 0,3 | 0,6 | 0,036 |
| 7,5 | 0,019 | 0,2 | 0,5 | –0,036 | 0,3 | 0,6 | 0,039 |
| 15 | 0,011 | 0,2 | 0,5 | –0,045 | 0,3 | 0,6 | 0,032 |
| 30 | 0,009 | 0,2 | 0,5 | –0,09 | 0,3 | 0,6 | 0,048 |
| 60 | 0,009 | 0,2 | 0,5 | –0,158 | 0,3 | 0,6 | 0,072 |
| 75 | 0,016 | 0,2 | 0,5 | –0,173 | 0,3 | 0,6 | 0,081 |
| 100 | 0,021 | 0,2 | 0,5 | –0,202 | 0,3 | 0,6 | 0,097 |
| CURRENT (A) | AVG ERROR % sin ϕ = 1i (90°) | LIMIT (%) [CLASS 1] | LIMIT (%) [CLASS 0.5] | AVG ERROR % sin ϕ = 0.5i (30°) | LIMIT (%) [CLASS 1] |
LIMIT (%) [CLASS 0.5] |
AVG ERROR % sin ϕ = 0.8c (– 53.13°) |
|---|---|---|---|---|---|---|---|
| 0,1 | 0,193 | 0,410 | –0,251 | ||||
| 0,5 | 0,024 |
3,0 |
2,0 | 0,079 | –0,044 | ||
| 0,75 | 0,018 | 3,0 | 2,0 | 0,070 | –0,032 | ||
| 1,5 | 0,006 | 2,0 | 1,0 | 0,047 | 3,0 | 2,0 | –0,027 |
| 3 | 0,008 | 2,0 | 1,0 | 0,052 | 2,0 | 1,0 | –0,017 |
| 7,5 | 0,003 | 2,0 | 1,0 | 0,071 | 2,0 | 1,0 | –0,032 |
| 15 | –0,006 | 2,0 | 1,0 | 0,023 | 2,0 | 1,0 | –0,03 |
| 30 | –0,002 | 2,0 | 1,0 | 0,095 | 2,0 | 1,0 | –0,034 |
| 60 | 0,004 | 2,0 | 1,0 | 0,154 | 2,0 | 1,0 | –0,052 |
| 75 | 0,015 | 2,0 | 1,0 | 0,187 | 2,0 | 1,0 | –0,056 |
| 100 | 0.027 | 2,0 | 1,0 | 0,224 | 2,0 | 1,0 | –0.042 |