TIDUF25A June 2023 – March 2025 ADS131M08 , MSPM0G1507
After performing power gain correction, perform the phase calibration. Similar to active power gain calibration, to perform phase correction on one phase, the other two phases must be disabled. To perform phase correction calibration, complete the following steps:
After performing phase calibration, calibration is complete for one phase. Gain calibration, offset calibration, and phase calibration must be performed for the other phases.
This completes calibration of voltage, current, and power for both phases. View the new calibration factors (see Figure 4-9) by clicking the Meter calibration factors button of the GUI metering results window in Figure 4-6. For these displayed calibration factors, the Voltage AC off parameter actually represents the active power offset (in units of mW) subtracted from each measurement and the Current AC offset parameter actually represents the reactive power offset subtracted (in units of mvar) from reactive power readings. Also, this shows example calibration factors for a meter that uses the two-voltage configuration. If the same meter is set for one-voltage configuration, the voltage and active power scaling factors are approximately half of what is in Figure 4-6, since the line-to-line voltage measurement is used for the voltage readings of both phases instead of measuring the two line-to-neutral voltages. Under the best conditions for a split-phase system, the line-to-line voltage measurement has an RMS value that is twice each of the two line-to-neutral RMS measurements, which means that the voltage fed to the ADC is also twice as much when measuring line-to-line voltage compared to when measuring line-to-neutral voltage. As a result, for one-voltage configurations, the voltage and power readings have to be divided by an additional factor of two, which is automatically done by following the active power and voltage gain calibration steps.
Figure 4-9 Calibration Factors
WindowView the configuration of the system by clicking on the Meter features button (illustrated in Figure 4-6) to get to the window that Figure 4-10 shows.
Figure 4-10 Meter Features Window