TIDUFB6 December 2024
The design uses four BQ78706 devices to monitor each cell voltage, monitor the temperature of a 52-cell battery pack, and to protect the pack against all unusual situations, including cell overvoltage, cell undervoltage, and overtemperature. In Figure 2-1, the top BQ78706 device is the BQ78706#4 and the bottom BQ78706 device is the BQ78706#1. The forward daisy-chain communication direction is from the BQ78706#1 device to the BQ78706#2 device.
Each BQ78706 has 11 GPIO pins for temperature sensing and 14 VC pins for voltage sensing. To monitor the temperatures for all the VC channels with fewer GPIO pins, two TMUX1308 multiplexers are used. The multiplexers expand temperature-sensing capabilities of one BQ78706 from 11 channels to 20 channels, which includes14 MUX-related thermistors, 2 constant resistors and 6 independent thermistors.
To run diagnostics for the TMUX1308 to prevent the MUX from failure mode, one channel of each TMUX1308 is connected to a constant resistor. This constant resistor is out of the range of thermistors which enable a plausibility check. This diagnostic method can show if the MUX is stuck on a specific channel or reporting voltages corresponding to incorrect channels.
The AVDD pin on the BQ78706 is used to supply power to the TMUX1308. Since AVDD can be configured as off state by shorting RX to AVDD, AVDD can enable a low shutdown current with no leakage current to external MUX devices. When BQ78706 is waked, then AVDD supplies all the external loads with 20mA capacity which is enough for MUX or other devices.
The internal passive cell balancing resistors can support up to 100mA of balancing current per channel. An odd and even cell balancing can be used to achieve average 50mA balancing current.
To isolate communication, the design uses two capacitors for daisy chain communication between two BQ78706 and two 1500V reinforced transformers in daisy chain communication between the BMUs or the BCU. This daisy chain communication enables a ring communication structure which can reduce gap current caused by daisy chain communication.
Besides daisy chain, CAN interface and MCU is also designed into this board. MCU MSPM0G3519 is used to collect the data from four BQ78706 devices and transfer data to the CAN bus. BQ78706 supports the universal asynchronous receiver-transmitter (UART) interface or serial peripheral interface (SPI) to the MCU. This design uses UART. Two-stage reinforced isolation is used to achieve 1500V insulation standard required creepage by both UL1973 and IEC 62477. The reinforced isolated power module is UCC33421 and digital isolator is ISO7731 which converts RX, TX and FAULT signals between BQ78706 and MSPM0G3519. To enhance the stability of the CAN interface communication, ISO6721 and UCC33420 are used for a functional insulation.
The power rail uses LM51406 to supply from a maximum 36VDC to 5VDC, which converts 5V to isolated power module.