TIDUFB6 December 2024
MCU and CAN interface is an optional choice to replace daisy chain. CAN interface is a widely-used standard interface. MCU MSPM0G3519 transfers the data from AFE1, AFE2, AFE3, and AFE4 to CAN interface. AFE1 works as a bridge device. The ISO7731 is used to connect the UART interface of the AFE1 and the MCU. A reinforced insulation is required since MCU is in low-voltage ground and AFE1 is in high-voltage ground. Two isolated stages are built with UCC33421 and ISO7731. Each stage has a 1500V working voltage and two stages are connected in series to meet 15mm creepage.
Since the TX pin of the BQ78706 supplies a constant voltage in both SHUTDOWN and ACTIVE modes, the ISO7731 is powered from the input (TX) when the BQ78706 SHUTDOWN mode of the ISO7731 is directly connected to BQ78706. A switch is added between BQ78706 and ISO7731 to prevent a leakage current. The switch can be a FET.
Figure 2-5 shows the MCU and CAN interface.
UCC33420 and ISO6721 provide a functional isolation for CAN interface. This CAN interface is usually connected to the CAN bus of BCU. The working current of the CAN transceiver, such as TCAN1044, is quite small. A functional isolation is set for the CAN transceiver not the MCU for a higher efficiency.