DLPU040B October 2016 – March 2023 DLP650LNIR , DLPC410
The Controller Board GUI uses a Script window to keep track of the images to be loaded and the commands to be executed on the DMD (#DLPU0406564). Once you’ve added an image and the commands you want to execute to the script, you can change the command order, delete and insert commands at a specified location within the script.
The application executes commands in the order in which the commands are entered in the script. For the application to execute commands, the first command in the script must be the Image command followed by the correct path and file name for an existing image. To learn how to insert an image into the script, see GUID-2709D377-9D7C-4E21-ADB9-916D5FAC48FE.html#GUID-2709D377-9D7C-4E21-ADB9-916D5FAC48FE.