DLPU040B October 2016 – March 2023 DLP650LNIR , DLPC410
The Reset command causes the mirrors to change from the current state to the state of that in memory. The contents of memory are determined by the Load or Clear commands. You can choose to reset all the blocks (Global), or you can choose to reset blocks individually using the Single Block option or a group of blocks using one of the Multiple Blocks options. Select the option you want to use and click the Add button to add the command to the script.