Use the following instructions to measure the inrush current during hot plug event:
- Set Jumper J4 position to desired slew rate as mentioned in Table 4-3.
- Set the input supply voltage VIN to 12 V and current limit of 10 A. Enable the power supply.
- Hot plug the supply between VIN and PGND points of connector J1.
- Observe the waveforms at VOUT (TP2) and input current with an oscilloscope to measure the slew rate and rise time of the eFuse with a given input voltage of 12 V.
Figure 5-2 and Figure 5-3 show the examples of inrush current captured on the TPS25946EVM eFuse Evaluation Board during hot plug event using TPS259460x and TPS259461x variants respectively.