Use the following instructions to observe USB
On-The-Go (OTG) performance:
- Set the input supply voltage to 5 V and
current limit of 10 A. Apply the supply between VOUT and PGND at connector J2.
- Connect a load of 200 mA between VIN
and PGND at connector J1.
- Turn on the input power supply at the
connector J2.
- Enable the eFuse by applying 1.5 V
externally between TP4 and GND. This external power supply is not required if the
EN/UVLO set point is above the voltage between TP1 and PGND before the device geting
enabled, which is the difference between the input supply at J2 and the voltage drops
across R1 and D1.
- Note that if the Power Good (PG) signal
is required to observe during this OTG mode of operation with 5-V input, the resistor R8
needs to be changed to 360 kΩ.
Figure 5-14 shows the
schematic to evaluate USB On-The-Go (OTG) port protection performance of TPS25946x
eFuse.
Figure 5-15 shows the power-up of
TPS25946x eFuse during USB On-The-Go (OTG) mode.