Use the following instructions to observe the transient overload performance:
- Place jumper J5 to an appropriate position to obtain required blanking period as per Table 4-3.
- Place jumper J6 in a suitable position to set required current limit as per Table 4-3.
- Set the input supply voltage VIN to 12 V and
current limit of 10 A and enable the power supply.
- Now apply an overload greater than the set
current limit (using the jumper J6) between VOUT and PGND for a time duration
less than the blanking period decided by using jumper J5.
- Observe the waveforms using an oscilloscope.
Figure 5-8 shows transient overload performance of TPS25946 eFuse on TPS25946EVM eFuse Evaluation Board.