Use the following instructions to
perform the output hot short test:
- Set the input supply voltage VIN to 12 V and current limit of
10 A. Turn ON the power supply.
- Short the output of the device for example, VOUT to PGND with a
shorter cable.
- Observe the waveforms using an oscilloscope.
Figure 5-12 and Figure 5-13
show the test waveforms of output hot short on the TPS25946EVM eFuse Evaluation
Board.
Note that it is very difficult to obtain repeatable and similar short-circuit
testing results. The following contributes to the variation in results:
- Source bypassing
- Input leads
- Board layout
- Component selection
- Output shorting method
- Relative location of the short
- Instrumentation
The actual short exhibits a certain degree of randomness because it microscopically
bounces and arcs. Ensure that configuration and methods are used to obtain realistic
results. Hence, do not expect to see waveforms exactly like the waveforms in this user's
guide because every setup is different.