SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
The device has a single voltage domain, VDDD. Within VDDD there are two power domains. The always-on AON domain and the switchable MCU domain. Throughout this documentation register mnemonics or descriptions can also reference the ULL domain, this is an alternative term for AON and is equivalent in all ways. Similarly the MCU domain can be described in register mnemonics or descriptions as SVT. See Figure 6-2 and Figure 6-3 for an overview of the voltage and power partitioning.