SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
There are three SYSTIM channels assigned to the radio. The radio receives compare events from the SYSTIM which are routed to the MDM, PBE, and RFE. These are used to trigger time start or stop commands. The radio can also be configured to output capture events to the SYSTIM, the selection of what event triggers the SYSTIM capture is done in the LRFDDBELL.SYSTIMOEV register. The normal use case is that RCL sets up and uses the SYSTIM interface.
If the radio is not in use (or not using SYSTIM interface), SYSTIM capture events can be captured from software by writing to the LRFDBELL.SYSTDMATRIG register.