Layout is very important to maximize the electrical and thermal performance of the total system. General guidelines are provided, but the form factor, board stack-up, and proximity of other components also need to be considered to maximize the performance. The parasitics in the board layout impacts the switching current in the MOSFETs and the output current of the device.
- VBUS traces should be as short and wide as possible to accommodate for high current.
- Minimize losses through connectors wherever possible, as the losses in these connectors will contribute a significant amount to the total power loss.
- Use vias under the exposed thermal pad for thermal relief.
- Place low ESR bypass capacitors to ground for VBUS, PMID, and VOUT. The capacitor should be placed as close to the device pins as possible.
- The CFLY pads should be as small as possible, and the CFLY caps placed as close as possible to the device, as these are switching pins and this will help reduce EMI.
- Connect all quiet signals to the AGND pins.
- Connect all power signals to the PGND pins.
- Do not route so the power planes are interrupted by signal traces.