SLOS879C April 2014 – June 2025 DRV2625
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The DRV2625 device has 8 parameters that control different aspects of modes of operation, namely: LRA_ERM, MODE[1:0], CONTROL_LOOP, TRIG_PIN_FUNC, AUTO_BRK_INTO_STBY, AUTO_BRK_OL, and LRA_WAVE_SHAPE. If any of these parameters are changed in the middle of a process execution (waveform playback, diagnostics or calibration), the DRV2625 interprets the change as an abort and goes into standby.
LRA_ERM parameter selects the actuator type.
MODE[1:0] selects between the 4 available process that can be run, namely RTP and Waveform Sequencer for waveform playback, diagnostics and calibration. The DRV2625 device is in standby state until a trigger is received. At that point the device executes the process selected in the MODE[1:0] parameter. Once finished, the DRV2625 device returns into standby state.
CONTROL_LOOP selects between open loop and closed loop.
TRIG_PIN_FUNC parameter selects the functionality of the TRIG/INTZ pin among the 3 possibilities: pulse trigger, level trigger and interrupt.
AUTO_BRK_INTO_STBY parameter enables automatic braking when going into standby. The DRV2625 device monitors the back-EMF of the actuator before going into standby, and if the back-EMF is moving, the actuator brakes and then go into standby. Note that for this function to be executed in open loop, the AUTO_BRK_OL pin must be enabled.
AUTO_BRK_OL parameter enables automatic braking for open loop mode. If enabled, every time a waveform is configured with a negative amplitude, the DRV2625 device brakes the actuator. This feature assumes that the actuator has been calibrated and works under closed-loop conditions.
LRA_WAVE_SHAPE parameter (available for LRA only) allows for selecting the waveform shape to be used when driving the LRA in open loop. In closed-loop this parameter is ignored.