9.3.2.1 Play a Waveform or Waveform Sequence from the ROM Waveform Memory
Initialize the device as listed in the Section 9.3.1 section.
Select the desired TRIG/INTZ pin function by changing the TRIG_PIN_FUNC parameter.
Identify the waveform index to be played and populate the waveform sequencer.
Trigger the waveform using the desired trigger method (GO bit, or external trigger). Note that if using the interrupt functionality, only the GO bit can be used to trigger the process.
Device automatically goes into standby upon
completion of the playback