SLDS274A September 2024 – March 2025 DRV81242-Q1
PRODUCTION DATA
When switching off inductive loads, the voltage across the power switch rises to VDS_CL potential, because the inductance intends to continue driving the current. The voltage at output pins is not allowed to go below VOUT_S_CL or VOUT_CL. The voltage clamping is necessary to prevent device damage.
The following figures show drawings of the clamp implementation. The maximum allowed load inductance is limited. The clamping structure protects the device in all operative modes (Sleep, Idle, Active, Limp Home).