The OLON bit can assume the following values:
- 0b = no Open Load at ON state detected, or the
channel is OFF when the diagnosis is performed
- 1b = Open Load at ON state detected
According to the setting of EN_OLON, different information are reported in the
Standard Diagnosis.
- EN_OLON set to 0010b to 0111b : The OLON bit
shows the Open Load at ON state diagnosis performed on the selected channel. The
information is updated at every Standard Diagnosis readout.
- EN_OLON set to 1010b : the OLON bit shows the OR
combination of all bits in OLONx register. The information is updated while the
diagnosis loop is running.
- EN_OLON set to 1111b : the OLON bit shows the
result of the latest diagnosis loop performed. Starting another diagnosis loop
to update the information is necessary.
- EN_OLON set to any other value: The OLON bit is
set to 0b. These values of EN_OLON bits are reserved and is not to be used in
the application.