SNVSCT1 October 2025 LM5066H
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
The LM5066Hx provides current limit protection with eight programmable thresholds ranging from 10 mV to 50 mV. Current limiting activates when the voltage across the sense resistor RSNS (between VIN_K and SENSE pins) exceeds the selected threshold. Two thresholds can be set directly using the CL pin, 25 mV when CL is connected to VDD and 50 mV when CL is connected to GND. The remaining six thresholds are available by programming the DEVICE_SETUP1 and DEVICE_SETUP2 registers through the PMBus interface.
During an over current event, the device offers two protection modes: over current blanking and current limiting. These modes can operate independently or sequentially based on configuration.
In over current blanking mode, the device allows the load current to flow without limiting it for a set time period, as long as it remains below the circuit breaker threshold (VCB). The LM5066Hx features two over current blanking thresholds with separate timers:
VCBL1 with timer tCBL1 for moderate over currents
VCBL2 with timer tCBL2 for higher over currents
These thresholds and timers are configured in the DEVICE_SETUP3 and OC_BLANKING_TIMERS registers. Typically, VCBL1 is set higher than VCL, and VCBL2 is set higher than VCBL1. For load currents between VCL and VCBL2, the tCBL1 timer activates. For load currents between VCBL1 and VCBL2, the tCBL2 timer activates.
The timer resets if the current drops below the respective threshold before it expires. If either timer expires due to prolonged overload, the device transitions to current limiting mode. In the LM5066H2, GATE2 turns off immediately when either timer expires. Over current blanking mode can be disabled by setting tCBL1 and tCBL2 to 0 μs.
In current limiting mode, the GATE voltage is regulated such that the current through MOSFET driven by GATE1 is limited to the set current limit threshold. The fault timer activates during current limiting. If the load current falls below the current limit threshold before the fault timer expires, normal operation resumes. If the current limit persists beyond the fault timeout period set by CTMR, GATE1 turns off. Current limiting can be disabled by setting bit 7 in DEVICE_SETUP3. When disabled, both GATE1 and GATE2 turn off after the blanking phase when either of the blanking timer expires. When a current limit fault occurs, the device sets fault flags in the STATUS_INPUT (7Ch), STATUS_WORD (79h), and DIAGNOSTIC_WORD (E1h) registers, and asserts the SMBA pin. SMBA signaling can be disabled using the ALERT_MASK (D8h) register.For reliable operation, the RSNS resistor value should not exceed 200 mΩ to avoid instability in the current limit control loop.
| Parameter | No. of Configurable Thresholds | Thresholds Values | Analog / Digital |
|---|---|---|---|
| Over Current Limit Threshold, VCL | 8 | 10mV, 12.5mV, 15mV,17.5mV, 20mV, 22.5mV and 25mV, 50mV | Analog |
| Over Current Blanking1 Threshold, VCBL1 | 4 | 1.25xVCL, 1.5xVCL, 1.75xVC, 2xVCL | Analog |
| Over Current Blanking2 Threshold, VCBL2 | 4 | 1.5xVCL, 1.75xVCL, 2xVCL, 2.25xVCL | Analog |
| Circuit Breaker Threshold, VCB | 4 | 1.2xVCL, 2xVCL, 3xVCL,4xVCL | Analog |
| Short Circuit Protection Threshold, VSCP | 1 | 1.5xVCB | Analog |
| Foldback Factor during StartUp | 3 | 0.05xVCL, 0.1xVCL | Analog |
| Over Current Blanking Timer1 | 16 | 0ms - 100ms | Digital |
| Over Current Blanking Timer2 | 16 | 0ms -10ms, 100ms | Digital |
| Circuit Breaker Blanking Time | 1 | 100us | Analog |
Regulation Timer (Constant Current Timer / P2t Timer) | Set with TIMER pin | Configurable using CTIMER | Analog |
| P2t Timer - Insertion Timer | 4 | 10ms – 100ms | Digital |
| P2t Timer - Retry Timer | 16 | 10ms – 10s | Digital |
| Watch Dog Timer during Startup/Retry | 16 | 10ms – 10s | Digital |